DRV.TEMPWTHRESH
Description
This parameter returns the over temperature warning threshold of the control circuit. The value is programmed in the drive and cannot be changed.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-05-00-000 |
|
General Information
| Type | Read Only |
| Units | degC |
| Range | N/A |
| Default Value | 85 |
| Data Type | Float |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2020 |
1 |
2020 (0x7e4) |
DRV.TEMPWTHRESH |
Signed32 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
DRV.TEMPWTHRESH |
2020 |
Float |
Read Only |
- |